Technical FAQs

Ask a Question

Osisense XC - 3D CAD file of the ZCY44 plastic roller lever

In the Traceparts library, this variable length plastic roller lever ZCY44, with pliable lever, does not exist. Please use the existing variable length plastic roller lever ZCY45, at following Telemecanique Sensors web site @
http://www.tracepartsonline.net/(S(0gchd4krqvepjyib4t5s52rl))/PartDetails.aspx?Class=TELEMECANIQUE_SENSORS&clsid=/F_TELEMECANIQUE_SENSORS/TELEMECANIQUE_SENSORS.010/TELEMECANIQUE_SENSORS.010.010/TELEMECANIQUE_SENSORS.010.010.020/TELEMECANIQUE_SENSORS.010.010.020.030/&ManID=TELEMECANIQUE_SENSORS&PartFamilyID=10-17052013-095091&PartID=10-17052013-095091&SrchRsltType=0&SrchRsltId=6
Difference between both levers is the lever material only. Same lever dimensions.
Was this helpful?
What can we do to improve the information ?