Technical FAQs

Ask a Question

Osisense XC - 3D CAD file of the ZCY46 steel roller lever

In the Traceparts library, this variable length steel roller lever ZCY46 does not exist. Please use the existing variable length plastic roller lever ZCY45, at following Telemecanique Sensors web site @
http://www.tracepartsonline.net/(S(0gchd4krqvepjyib4t5s52rl))/PartDetails.aspx?Class=TELEMECANIQUE_SENSORS&clsid=/F_TELEMECANIQUE_SENSORS/TELEMECANIQUE_SENSORS.010/TELEMECANIQUE_SENSORS.010.010/TELEMECANIQUE_SENSORS.010.010.020/TELEMECANIQUE_SENSORS.010.010.020.030/&ManID=TELEMECANIQUE_SENSORS&PartFamilyID=10-17052013-095091&PartID=10-17052013-095091&SrchRsltType=0&SrchRsltId=6
Difference between both levers is the roller material only. Same roller dimensions.
Was this helpful?
What can we do to improve the information ?