Browse FAQs

Is NSX R/HB1/HB2 line load reversible?

Published date: 11 September 2018

All R, HB1, and HB2 circuit breakers are restricted for use as line-load connection. They can not have power fed into the bottom of the circuit breaker.
They will be marked with Line and Load markings. If reverse feeding is required the configuration has to be validated by testing.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.