Technical FAQs

Ask a Question

Osisense XC special - Need a XCRT215 limit switch for conveyor belt shift monitoring, to be used at high temperatures up to +150°C

The XCRT215 limit switch for conveyor belt shift monitoring, is qualified to be used in a maximum ambient air temperature of +70°C. If the function need is a maximum temperature of +150°C instead of +70°C, please propose the HL525WD* similar limit switch able to resist to +350°F (Farenheit) = 176.6°C (Celsius). Please refer to the "Severe Duty Mill and Foundry - limit switches" catalog in SquareD brand for the product selection. Example of data sheet in the following @ http://www.tesensors.com/global/en/product/limit-switches/nema-limit-switches/?cat_id=BU_AUT_61349_L3&conf=sensors&el_typ=product&prd_id=HL525WDL2M57&scp_id=Z000
Was this helpful?
What can we do to improve the information ?