Technical FAQs

Ask a Question

What is maximum voltage allowed on DO5 on a TM171ODM22R

The Maximum allowed voltage on Digital Output 5 (DO5) of  TM171ODM22R is +12Vdc & usage of +12Vdc from controller is recommended.
Was this helpful?
What can we do to improve the information ?