Technical FAQs

Ask a Question

Can the HMIG5U function without front panel connected to it?

Issue:
Can the HMIG5U be used without front panel connected to it?

Product Line:
HMIGTU, Front Display, HMIDT

Environment:


Cause:


Resolution:
No, it can not.  It needs the front panel to power up the unit..  A possible solution would be to go with the Magelis HMIBSO or HMIBSU Box PC
Was this helpful?
What can we do to improve the information ?