Technical FAQs

Ask a Question

Osisense XC special - Dimensions of the screw limit switch XR2AA03K20

Attached XR2AA02K* or XR2AA03K* dimensions from catalog with some additional data (the chain sprocket XR2AZ2 fitted is not delivered with the standard XR2AA switch).

Was this helpful?
What can we do to improve the information ?