Browse FAQs

How to access SCADA Alarms using a third party OPC A&E Client

Published date: 27 March 2019

Issue
Using a third party OPC A&E Client to access Alarm Server data (OPC A&E Server).

Product Line
PowerSCADA Expert (all versions)

Environment
OPC A&E (Alarms and Events) Client

Cause
You can use a third party OPC client application, such as Matrikon, to access your system and view alarm server data.
To register your alarm server (in your OS) you need to have administrative privileges.

Resolution
To allow the third party application access: 

1.  Select the project and run the Computer Setup Wizard.

2.  On the General Options setup dialog select 'Register' . The Alarm server for that project is then registered and available for access via the third party application.




3.  Run the third party application. From the list of available servers select Serck.ScxV6OPCAE.<AlarmServerName>.<IP address>

4.  Connect to the Server and depending on your third party application Create Event Subscription

All events will be listed. Runtime does not need to be restarted after this change. 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.