Technical FAQs

Ask a Question

Which terminals of the vigirex toroids are used to connect to the monitoring / protection relay?

On the Vigirex toroids are located three terminals marked 1, 2 and 3. The connection must be made as follows:
terminal 1 --> T1
terminal 2 --> T2
terminal 3 --> not used for the connection.
Was this helpful?
What can we do to improve the information ?