Technical FAQs

Ask a Question

PME Web Reports 'Download as an Excel Document' prompts the following error: "The file is corrupt and cannot be opened."

When attempting to download a generated report via web applications as an 'Excel Document', the following error is observed by Microsoft Excel: "The file is corrupt and cannot be opened."

Product Line
Power Monitoring Expert 8.2
Ecostruxture Web Services

Power Monitoring Expert
Microsoft Excel 2010, 2014 & 2016

The Microsoft Office Trust Center contains security and privacy settings to protect the system from potentially dangerous files.

1. Run Microsoft Excel.
2. Click on File > Options.
3. Select Trust Center > Trust center settings.
4. Select Protected view.
5. Uncheck all the options under Protected View > OK.

6. Restart Excel and try to open Excel documents.
Was this helpful?
What can we do to improve the information ?