Technical FAQs

Ask a Question

What is the difference between BMXXTSCPS10 and BMXXTSCPS20

Power supply modules are supplied with one 5-pin screw terminal and one 2-pin screw terminal block, part number BMXXTSCPS10. Furthermore two kits are on sale:

BMX XTS CPS 10 kit which contains the following equipment:
- one 5-pin screw terminal block
- one 2-pin screw terminal block
- one guidance system (only for AC and 125 VDC modules)

BMX XTS CPS 20 kit which contains the following equipment:
- one 5-pin spring terminal block
- one 2-pin spring terminal block
- one guidance system (only for AC and 125 VDC modules)
Was this helpful?
What can we do to improve the information ?