Technical FAQs

Ask a Question

EMC Investigation Case Study

Goals and Symptoms
The purpose of this resolution is to provide the 'EMC Investigation Case Study' that was performed on a finalized
control system installation.

Facts and Change
All PAC hardware

Causes and Fixes
The objective of this EMC investigation was to determine if possible interrupts to the control system operation may have
been due to possible excess EMC conditions. This investigation has been carried out on a finalized installation. Results
shown in this report are based on the installation status during a maintenance shutdown

To obtain the case study, download the attched file named 'EMC Investigation Case Study 1.6.pdf  '.
Was this helpful?
What can we do to improve the information ?