Browse FAQs

What is the Schneider Electric part number for the 6 pin cable-side motor connector for BRS3 and VRDM3 three phase stepping motors?

Published date: 03 October 2018

The connector that is found on the end of the motor power cable and mates to the motor connector has a part number of 62501504001 and is available as a spare part.

The connnector will comes with solder type pins.

 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.