Technical FAQs

Ask a Question

Can ATS work with IE3 motor?

Yes, it can, but there is a limitation.

IE3 (premium efficiency) motor needs higher starting current to generate sufficient torque than IE2 or IE1 motor. Exact value depend on specific motor. Depends on application oversizing of ATS to be able to provide sufficient starting current can be required.
Was this helpful?
What can we do to improve the information ?