Browse FAQs

Osisense XC - How is the XCRT315 switch mounted

Published date: 25 September 2019

Please refer to the specific instruction sheet of the XCRT315 switch for conveyor belt shift monitoring, providing the installation rules, supplied with the product and available on our website at following @ http://download.schneider-electric.com/files?p_Doc_Ref=130514501A55
In addition we can show the blind holes details used to fix the unit by two M5 screws with cylindrical head dia 8.5...9.5mm. The 2 blind holes are accessible after removing the cover having the roller arm.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.