Technical FAQs

Ask a Question

Does the IFE ethernet module support the SNMP protocol?

Issue:
Does the IFE ethernet module support the SNMP protocol?

Product Line:
Enerlin'X Ethernet Interface IFE (LV434011 and LV434010)

Environment:
communications protocols

Resolution:
The IFE module supports the SNMP protocol strictly to report information from the unit itself to a Network Manager System. It is not designed to collect data from sub devices, or to be used as a SNMP to Modbus gateway.
Was this helpful?
What can we do to improve the information ?