Technical FAQs

Ask a Question

How to Change Stale Data Settings in MDI for Logged Data

A device using a tranlator is setup for logging in MDI.  The report shows some entries are blank and no data is captured.

Product Line
Power Monitoring Expert, PME

Modbus Device Importer, MDI

Logged data behavior in case the device looses communication and goes into stale mode.

There are two settings that control how logged data behaves in case the device goes into stale mode:

The options for when data is stale are:
    - log an empty row
    - use last known value

The settings can be changed in MDI by clicking on 'All' in the 'Configure Logging and Calculation' section:

Was this helpful?
What can we do to improve the information ?