Technical FAQs

Ask a Question

Where can I download Power Monitoring Expert 8.0 installation files?

Issue
The installation files for Power Monitoring Expert 8.0 (PME 8.0) are needed

Product
Power Monitoring Expert 8.0 (Base, Health Care, Data Centers, and Buildings)

Environment
Software Installation Files

Resolution
PME 8.0 (ISO) software can be found at the Schneider Electric Box links below: (Note as of 6/7/2017, the latest version of PME is 8.2, the installation files can be downloaded from article FA312664)
 
PME 8.0 Base https://schneider-electric.box.com/s/scva5084kic36rayrztph2cr8mguofcm
PME 8.0 Healthcare https://schneider-electric.box.com/s/njm5wd8temkecypkp0d8eda5vyet2th7
PME 8.0 Data Center https://schneider-electric.box.com/s/7pgh4yup0i3r4qli6exi38hx57z24d9k
PME 8.0 Buildings https://schneider-electric.box.com/s/44lsdd0acqsmeyxmx2xmruhvcpmtoi5i

Note: If there are issues accessing the above links, please try removing the secure encryption by removing the s in https. For example, the first link would become http://schneider-electric.box.com/s/scva5084kic36rayrztph2cr8mguofcm

For PME 8 Documentation, refer to article FA317837
Was this helpful?
What can we do to improve the information ?