Browse FAQs

What causes a "11687 TCP/IP machine in a bad state" error when using the Concept simulator?

Published date: 29 November 2018

                                               
11687    TCP/IP machine in a bad state

1/  This error can occur if there are XXMIT or XMIT blocks in the project. Delete the blocks and redownload if using the simulator.
2/  Another device with the same IP address?
3/  Corrupt Winsock.exe or Ethernet NIC driver?

 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.