Technical FAQs

Ask a Question

L525 Mill & Foundry switches - Picture of the roller lever arm AL1650

Attached picture of the roller lever arm AL1650 using a Nylon roller. The AL1650-1 is the same lever arm with a Teflon roller for high temperatures. The AL1802 roller lever arm is similar to the AL1650; the lever arm is longer (3.0 inches instead of 2.31 inches)

Was this helpful?
What can we do to improve the information ?