Technical FAQs

Ask a Question

Preventa XY2C - Can the XY2CED rope pull switch be used with vertical cables?

Because of the switch design using 2 cables in equilibrium, the XY2CED cannot operate with vertical cables. The XY2CED switch can operate properly only in the conditions precised into the instruction sheet supplied with the product, without any cable deflection : The installation must be horizontal and rectilinear. The installation vertical is forbidden.

Was this helpful?
What can we do to improve the information ?