Browse FAQs

What additional revenue firmware security features are available in PM8000 series meter ?

Published date: 20 December 2018

Issue:
User would like to know what additional revenue firmware security features are available in PM8000 meters

Product Line:
PM8000 Meters

Environment:
Meter Security 

Cause:
The PM8000 meter has additional firmware security features.

Resolution:
Below are the additional firmware security  features:

• You can only upgrade to revenue-qualified firmware and frameworks.
• Your firmware upgrade files have digital signature confirmation to help ensure
firmware authenticity.
• You cannot perform resets or configure some revenue-specific parameters on
your meter while it is revenue-locked.
• Your firmware upgrades are recorded in your meter’s event log. An additional
firmware upgrade log is stored on your meter. Contact technical support for
information on upgrade log retrieval. Tech support can be reached by dialing 1-888-797-6468. 

 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.