Browse FAQs

In Ecodial Advance Calculation, what is the minimum cross section area of the PE conductor ?

Published date: 19 October 2018

As per the IEC 60364-5-54 standard, below table give the details of PE conductor size
 
Cable PE type Live Conductor Minimum Cable Cross section area
Copper Separate PE Multicore 4 Sq.mm
Copper Included PE Multicore Same as Phase cable cross section area
Copper Separate PE Single core 4 Sq.mm
Aluminum Separate PE Multicore 16 Sq.mm
Aluminum Included PE Multicore Same as Phase cable cross section area
Aluminum Separate PE Single core  Sq.mm

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.