Browse FAQs

How to reset Peak Power Demand values from the front display of CM4000

Published date: 28 September 2018

Product Line
CM4000 series

Environment
Keys on the front display.

Resolution
To reset the accumulated Peak Power Demand values, follow the procedures below:

  1. From the Front Panel Main Menu, select Resets
  2. Select Demand. The password prompt displays.
  3. Select your password. The default password is 0.
  4. The Reset Demand Screen displays. Select the value that you need to reset. 
  5. Press Enter on the selected option. The "No" option starts to blink
  6. Use the Up arrow to change to "Yes", then press Enter. The "Yes" will stopp blinking
  7. Press the Menu button. You will get a confirmation that the Reset was complete. 
  8. Press the Menu button two more times to return to the Main Menu Screen

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.