Technical FAQs

Ask a Question

The ATV32 and ATV320 multipoint keypad function only works with certain versions of VW3A1101 keypads.

Issue:
The ATV32 and ATV320 multi-point keypad function only works with certain versions of VW3A1101 keypads.

Product Line:
ATV32 and ATV320

Environment:
All 

Cause:
Certain versions of the VW3A1101 keypad will work with the multipoint 

Resolution:

I test ATV320C and also ATV32 the keypad versions below:

- CPU V1.2IE07  FlashSoft V1.1IE26. --> OK
- CPU V1.2IE12  FlashSoft V1.1IE28. --> OK
- CPU V1.2IE12  FlashSoft V1.1IE29. --> OK
- CPU V2.5IE21  FlashSoft V1.1IE33. --> OK

When you connect the keypad, you will see Connection in progress, you should push the main button "ENT", to see the multi-point menu, then select the drive with address of each one, then the keypad will displays the all drives.

This function will not work with the VW3A1111 keypad displays. 


 
Was this helpful?
What can we do to improve the information ?