Technical FAQs

Ask a Question

Is there a System Word which will tell us the percent of program fragmentation?

No. There is not a %SW which will provide a fragmentation percentage or %S which would indicate the need for a PACK command.
There is an red icon in the form of an SD card that will appear in the lower right of your Unity screen when the need to Packarises.



R-2122018

 
Was this helpful?
What can we do to improve the information ?