Technical FAQs

Ask a Question

Osisense XU - Pitch of the M18 thread in the XUB5BPANM12 photoelectric sensor

The pitch of the M18 thread in the cylindrical case of the XUB5BPANM12 photoelectric sensor is 1mm (M18x1mm). Such data is valid for all the XU photoelectric sensors in dia18mm (plastic or metal).


 
Was this helpful?
What can we do to improve the information ?