Technical FAQs

Ask a Question

Can one replace the soft charge resistors on the AV5000 without replacing the contactor?

Issue
AV5000's soft charge resistors needs to be replaced with the contactor intact. 

Product Line
AV5000

Resolution
The soft charge resistors and the contactors are packaged together and it's recommended to replace both the contactor and resistors. Refer to the attached document for further information. 
Was this helpful?
What can we do to improve the information ?