Technical FAQs

Ask a Question

Video: How to obtain a URL for sharing a PME Slideshow

Issue
Getting a URL to share a Slideshow in PME.

Product Line
EcoStruxure™ StruxureWare Power Monitoring Expert 8.2 (PME 8.2)

Environment
PME Web Application Dashboards Slideshow

Cause
Provide remote viewing capabilities for a PME slideshow.

Resolution
In order to obtain a URL for a specific PME slideshow:

1. Open PME web application and select the Dashboards tab

2. Click on the Slideshow Manager icon  (listed on the right side under 'Dashboard Library')

3. Click on a previously saved slideshow, then click Share to open the 'Share Slideshow URL' dialog as shown below:

     

    The dialog includes the URL for the slideshow, which you can copy and distribute so that others can access the slideshow.

4. Copy and share the URL

NOTE: The client browser must have access to the URL to view the slideshow. (Do not use 'localhost' in the URL)

Was this helpful?
What can we do to improve the information ?