Technical FAQs

Ask a Question

How to resolve the issue with the Magelis HMIBM/PSO/PSP touchscreen intermittently stops responding.

Issue:
How to resolve the issue with the Magelis HMIBM/PSO/PSP touchscreen intermittently stops responding.

Product Line:
HMIBM, HMIPSO, HMIPSP, PenMount, Water Function

Environment:


Cause:


Resolution:
A work around would be to unzip the attached PCIMset, launch the executable PenMount file, and uncheck the water function.  See below illustration:

Was this helpful?
What can we do to improve the information ?