Browse FAQs

Can you invert the CT polarity of the EM35xx series meters?

Published date: 28 January 2019

Issue:
The CT's are wired incorrectly for an EM 35xx series meter and a customer would like to correct the issue by inverting the polarity through the meter front panel or software similar to an ION meter.

Product Line:
EM35xx series meter

Environment:
CT wiring

Cause:
The CT's for the meter have been wired incorrectly.

Resolution:
The CT polarity is not changeable either from the front panel, software configuration, or register writes so the meter will have to be deenergized and rewired correctly.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.