Technical FAQs

Ask a Question

Activation of remote debugging for SCADAPack 570 & SCADAPack 575 Logic

Issue

By default, only DNP3/IP communications are activated on the device. To be able to debug SCADAPack x70 Logic, Logic Debugger Service has to be enabled.

Product Line

SCADAPack 570 & SCADAPack 575

Environment

Remote Connect, SCADAPack x70 Logic Editor

Resolution

To activate Ethernet access for debugging purposes:

1. On the Configuration tab, select IP Communication > Services:

2. Select the Logic Debugger checkbox
3. Click Apply and Write Configuration to Device
 
      When the box is checked, you can use Ethernet to connect to the SCADAPack x70 logic applications on the device for debugging purposes.
An Ethernet connection allows remote access to the logic applications.

When the box is not checked, you can only use USB to connect to the SCADAPack x70 logic applications on the device.
A USB connection allows only local access to the applications. You may want to limit users to local access for reasons of safety, security, permissions or administrative policy. 

Default: Unchecked
Was this helpful?
What can we do to improve the information ?