Technical FAQs

Ask a Question

How is the EIP Slave Adapter capability of a BMXNOC0402 module setup?

Title
BMXNOC0402 EIP Slave Adapter capability

Issue
Need procedure to configure the EIP Slave Adapter capability of a BMXNOC0402 module.
 
Product Line
Modicon M340 

Environment
ODVA Ethernet/IP 
 
Cause
User configurable capability.
 
Resolution
The BMXNOC0401 supports up to 3 instances of local slaves (Local Slave 1, Local Slave 2, and Local Slave 3).

To Access settings:

  1. Double-click the BMXNOC0401 master communication DTM in the Unity Pro DTM Browser.
  2. In the navigation tree on the left side of the Device Editor window expand the EtherNet/IP Local Slaves.
  3. Select one of the three available local slaves.
To Configure parameters:
  1. Enable the local slave under the Active Configuration box.
  2. Specify the size of the local slave input and output assemblies.
Was this helpful?
What can we do to improve the information ?