Technical FAQs

Ask a Question

Osisense XC_Where are indicated the commercial ref. and the date code on the XCKMR or XCKVR switches, when they do not figure on the front cover

On the XCKMR or XCKVR switches for hoisting applications, the commercial reference and the date code are normally indicated in the product label, marked on the front cover. The date code, or production date, is indicated like that : Plant code - Year - Week. When such data do not figure on the front cover, please check on the product side the little label separated from the main label, providing these data. See attached picture.

Was this helpful?
What can we do to improve the information ?