Technical FAQs

Ask a Question

ADVC Recloser Hot Line Tag functionality not going active

The customer is testing the ADVC Recloser and is going to the local control panel and setting Auto Reclose to OFF. From here, they press the Hot Line Tag button. When the Hot Line Tag button is pressed, the corresponding light does not light up and the log files show that the Recloser was never set to Hot Line Active.

Product Line:
ADVC Recloser

ADVC Recloser

There are a 2 things that would prohibit Hot Line Tag from being applied:

- Switchgear not available 
- Battery Low 

Ensure that Switchgear is connected and showing as available in the ADVC Controller. Also ensure there are no Battery Low errors in the ADVC controller.
Was this helpful?
What can we do to improve the information ?