Technical FAQs

Ask a Question

Osisense XC - Difference between the XCRF17 and the XCRF171 limit switches for hoisting

The alone difference between the XCRF17 and the XCRF171 limit switches for hoisting is the degree IP of protection according to the IEC 60529 standard.
XCRF17 = IP54; data sheet @ http://www.tesensors.com/global/en/product/limit-switches/xc-special/?cat_id=BU_AUT_2593_L4&conf=sensors&el_typ=product&prd_id=XCRF17&scp_id=Z000
XCRF171 = IP65; data sheet @ http://www.tesensors.com/global/en/product/limit-switches/xc-special/?cat_id=BU_AUT_2593_L4&conf=sensors&el_typ=product&prd_id=XCRF171&scp_id=Z000
Was this helpful?
What can we do to improve the information ?