Technical FAQs

Ask a Question

Windows 10 PRO version 1607 can't verify Schneider Driver digital signature.

With Windows10 PRO the last PLCUsb driver version V3.12 IE22 (PLCUsb Driversuite 14.9.0.0) is not installed due to a digital signature issue. This information is available going on BMXCPU properties.

A new PLCUsbdriver release solving this issue will be available soon.
Waiting this date, it is possible to go over disabling option Secure-Boot in the UEFI-BIOS.

 
Was this helpful?
What can we do to improve the information ?