Technical FAQs

Ask a Question

Can Ecodial Advance Calculation versions be installed in Virtual machine or windows 10?

No. Virtual machine and windows 10 environment are not tested and it is suggested to use windows 7 or 8 for Ecodial Advance Calculation .
Was this helpful?
What can we do to improve the information ?