Technical FAQs

Ask a Question

How to export solution table in Ecodial Edvance Calculation?

Create and calculate network. Click on the solution table button at left bottom corner, possible to see all the components solutions. Click on the Export option and select whether only selected solution tab to be exported to excel or all solution tabs. Export to excel & save it in the local computer.
Note:  If there are errors existing in the network calculation then it is not possible to export solution table.
Was this helpful?
What can we do to improve the information ?