Technical FAQs

Ask a Question

How to make operating modes in Ecodial Advance Calculation?

Please follow the following steps to make different operating modes
1. By default "Normal operating mode" will be created & further to create different operating modes select operating mode drop down option.
2. Click on the 'management of operating modes' 
3. In the mmanagement of operating mode window select "duplicate this mode" , enter the name of the new operating mode , enter the comments if any and close the window.
4. Now in the design and sizing tab it is possible to see new operating mode& adjust the load and source as per the requirement.
Was this helpful?
What can we do to improve the information ?