Technical FAQs

Ask a Question

ION7650 Anti-Tamper Sealing Kit Installation

Issue
Installing anti-tamper sealing kit

Product Line
ION7650

Environment
Installation/Setup

Cause
The meter incorporates two sealing cans and two sealing bars through which traditional lead/wire seals can be inserted. When utilized, these lead/wire seals help prevent unauthorized personnel from gaining access to internal meter components.

Resolution
The following image describes how to install the anti-tamper sealing kit.
Was this helpful?
What can we do to improve the information ?