Technical FAQs

Ask a Question

Osisense XU - What is the difference between XUK9TAH2MM12 and XUK9TAH2MM12S78

The XUK9TAH2MM12S78 photoelectric sensor for distance measurement is an adapted sensor. It is in fact the standard XUK9TAH2MM12 preadjusted in factory at the following analog output values : 4mA = 300mm and 20mA = 35mm. Logistic situation in 2017 : XUK9TAH2MM12S78 is available to order, sales open for all customers, manufacture at order reception.
Was this helpful?
What can we do to improve the information ?