Browse FAQs

How can I correct Proworx 32 error 'Decompressor error #1'?

Published date: 06 December 2018

Decormpression Error #1 indicates that the User does not have complete Administrator rights to the PC.
Right click on the Proworx 32 desktop icon or go to the executable Properties - Security.
Make sure that the User has Full control, Modify, Read & execute,  Read, and Write permissions.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.