Technical FAQs

Ask a Question

Preventa XCS - Are the ​XCSRC RFID contactless safety switches, single and series models, compatible with the compact safety controller XPSMC

The ​XCSRC RFID contactless safety switches, single and series models, are perfectly compatible with the compact safety controller XPSMC. The OSSD's pulse width, during the OSSD monitoring by the XCSRC RFID contactless safety switch, is not detected like a stop signal by the XPSMC unit. The short circuit detection in the XCSRC cabling is detected by this OSSD monitoring.

        
Was this helpful?
What can we do to improve the information ?