Technical FAQs

Ask a Question

Preventa XCS - Connection diagram of the ​XCSRC*0M12 RFID contactless safety switch, single model, to the safety controller XPSMCM

Attached the connection diagram of the ​XCSRC*0M12 RFID contactless safety switch, single model, to the safety controller XPSMCM. The single model is a basic model, without manual start & EDM embedded (external device monitoring). It is dedicated to a point to point connection to some XPS safety interface (relay, controller, PLC ...). The manual start & EDM loop is connected to the XPS safety interface. The external KM1 and KM2 contactors must have force-guided contacts or NC mirror contact.

Was this helpful?
What can we do to improve the information ?