Technical FAQs

Ask a Question

Preventa XCS - Wiring diagram of the ​XCSRC*1AM12 RFID contactless switch, standalone model with a non monitored start

Attached the wiring diagram of the ​XCSRC*1AM12 RFID contactless switch, standalone model with a non monitored start. It is possible to cancel the start button to get the automatic start. The XCSR standalone model does not need some safety relay or safety interface XPS type.
Was this helpful?
What can we do to improve the information ?