Technical FAQs

Ask a Question

Preventa XCS - Wiring diagram of the ​XCSRC*1MM12 RFID contactless safety switch, standalone model with monitored start

Attached the wiring diagram of the ​XCSRC*1MM12 RFID contactless safety switch, standalone model with monitored start. It is not possible to bypass or cancel the start button. The XCSR standalone model does not need some safety relay or safety interface XPS type.
Was this helpful?
What can we do to improve the information ?