Browse FAQs

Do I need the Modbus Plus Driver Suite with the XBTZGUMP?

Published date: 16 August 2019

Yes, the Modbus Plus Driver suite is required. It does not require registration

It is included with the Vijeo Designer Disk.

The configuration for the XBTZGUMP is done in the Vijeo Designer software.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.