Technical FAQs

Ask a Question

What do the crash codes mean in MBX Demo for the Modbus Plus MBX Driver Suite?

Occasionally, due to adapter card malfunctions, the MBX Driver may detect an adapter card fault. In most cases, this is due to electrical interference, either internal or external to the computer system. However, it can also be an indication of a card failure. The MBX Driver tries to recover from these failures automatically.
Every time a fault condition is detected, an internal adapter fault counter is incremented and the last crash code is recorded internally. Both of these numbers can be viewed through the Device Information screen of the MBX Demo program. The following is a complete list of all crash codes that can aid in diagnosing these types of problems.
Was this helpful?
What can we do to improve the information ?