Technical FAQs

Ask a Question

Preventa XCS - Wiring example of the ​XCSRC*1AM12 RFID contactless safety switch, with automatic restart

Please refer to the attached file showing the standalone model references to select and the corresponding wiring diagram. With the monitored start references XCSRC*1MM12, the automatic start with an electrical jumper to bypass the "start button" does not operate, because the switch reader is waiting for the release of the start button after activation in a time window of 5 secondes. The button is really monitored so you cannot bypass it.
Was this helpful?
What can we do to improve the information ?